Part Number: TPS65988
Other Parts Discussed in Thread: TPS65987D
I am trying to understand how to setup a TPS65988 for use with a USB type A connector on Port 2 utilizing what features and protocols allow for it in said part.
The hardware design is based on the TIDA-01515. Hardware is completed and I am successfully able to program my board using the Application Customization Tool.
Found document: SLVAE17A TPS65987D and TPS65988 BC1.2 Implementation Guideline
While interesting, the instruction to change certain registers is somewhat confusing and of no real help at all.
What I require is a step by step instruction how to change the required registers using the Customization tool.
To add, while the Tida-01515 is a great hardware design start point, why is there not some project available to this specific design to assist development. Such a project would be invaluable and speed up development substantially. If somebody has such a project to share, it would be greatly appreciated.
Thank you