Hi Team,
Could you please help with below several quick questions regarding DS90UB941, the structure is to use DS90UB941+2 DS90UB948 to connect to 2 Display.
1. Is 941 able to support different resolution with different frame rate? For example, 1920x720/30fps for cluster and 1024x728/60fps for IVI?
2. Normally customer will set the GPIO as outputting remote data to reflect if any remote display being touched. In this case 941 is connecting to 2 touch screen, question is that how to configure GPIO to map to different remote FPDLINK back channel so the local SOC can tell which screen is being activated?
Thanks