Part Number: DP83TC811S-Q1
Hi Team,
My customer now use DP83TC811S-Q1 and met some issue when doing RI test.
In RI test ,At the range of 1.9~ 2.3Ghz, pin communication is abnormal (completely lost the package). When interference are removed, pin communication immediately returned to normal.
- PHY's clock and T1 working frequency are very low. However the interference signals is nearly 2GHz, which should not have an impact on PHY and cause communication problems. So why communication is abnormal.
- Is there any way to read the state of PHY when it works abnormal so that we can locate where the problem is?
Thanks!