This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: DUT RE EMI Test exceed 4dB @1.6GHz

Part Number: DS90UB933-Q1

Hi Team,

It is really hard time to deal with customer's EMI issue for me these days...

Their DUT has both 933 and 934.

Based on the effort before, customer eventually passed the RE test at the range of 30M-439MHz.

However, it failed in 1603.9MHz (exceed nearly 4dB @1.603GHz)...Which is the 51*PCLK (31.45MH*51=1603.95MHz)

Could you please give some advice or guidance? Many thanks in advance!