Part Number: TPD2EUSB30
Other Parts Discussed in Thread: ESDS314, TPD4E05U06, TPD4E1U06, ESDS304, TPD2E2U06
Hi team,
I am looking for a transient voltage protection for SGMII CML lines (1.25Gbps + 100ppm), rise time is 60 to 300ps. Total jitter must be less than 192ps.
The interface goes between two ethernet switch chip. there was a TI part that was used for USB3.0 that worked out very well. What can you recommend?
The SGMII lines are differential CML lines and there are only two pairs. I was also considering the USB3.0 protection parts TPD2EUSB30. Will this work?
would the TPD4E1U06 or TPD4E05U06 work too?
Thanks,
Kevin