Hi Expert,
Please tell me about the method of termination for unused pin .
Conditions:
-There is power supply to the device.
・ Input Low to / PDWN
・ There is no transmitter connection, only the terminal 100Ω connecting each +/- input
1. The LVDS input pins of RxIN0 to RxIN3 and RxCLKIN will float, is that OK?
2. According to the specifications "7.1 Overview", the following is stated, so if you set / PWRDWN to Low, customer understand that it is okay even if there is no valid data input.
"These devices feature a PWR DWN pin to put the device into low power mode when there is no active input data."
At this time, RxOUT0 ~ 27 seem to be Low, what is the value of pull-down resistance ?
3. Does the power consumption in the power down mode typ = 140uA include the current when the input is floating or the output pin is pulled down?
4. When only the device power at the transmitter is shutdown, is there a possibility that the leakage will come from the receiver to transmitter?
Also, if the / PWRDWN = Low is set at that time, will the leakage be eliminated?
Thanks
Muk