Part Number: DS90UB947-Q1
Hi team,
I have several questions about GPIOs of 947:
1. How many GPIOs can be used for bidirectional control signal? (GPIO0-GPIO3, D_GPIO0-D_GPIO3 ? )
2. Does the use of D_GPIO only need to be used under dual link mode? Does it have anything to do with the number of DSI connected to the input (eg. DSI inputs only D0-D3 connected ).
3. Can the usage of D_GIPO be equivalent to general GPIO in dual link mode? Except for faster speed.
Thanks for your patient to reply for these question.
Best regards,
Ansel Song