Part Number: DS125DF1610
Hi,
please check attach file.
Thanks
cannieds125df.docx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Regarding: "How to setup reg 0x96 bit 5? Do 6A,6B,7A,&b all master?"
Regards,
Rodrigo Natal
HSSC Applications Engineer
Hi,
at datasheet page 17. it seem one master others are slave. If I setup all as master, does it will has any impact?
Br,
cannie
The cross point switch can also be used to replicate data or perform a broadcast function. The options for this
type of configuration include:
• 1:2 – any channel input to any 2 channels output
• 1:3 – any channel input to any 3 channels output
• 1:4 – any channel input to all 4 channels output
When the cross point switch is configured to replicate/broadcast data a master must be assigned during the
cross point configuration. The master channel will have control over the CTLE adaption. All of the slave channels
will be able to adapt their own DFE, but will not have control to adapt the CTLE. In this type of configuration there
must be 1 channel assigned as a master. All other channels in the broadcast network must be assigned as
slaves. There cannot be more than one master channel in a broadcast network. In a broadcast configuration, the
straight through path connecting the broadcasting input to its own output needs to be enabled and set to have
Hi,
Setting all channels to master will not have any negative impact, as this is our recommended setting as called out in the datasheet register table (see below.) My apologies for the confusion. The slave option is no longer supported.
|
Address (Hex) |
Bits |
Default Value (Hex) |
Mode |
EEPROM |
Field Name |
Description |
|
96 |
7 |
0 |
RW |
N |
RESERVED |
|
|
6 |
0 |
RW |
N |
RESERVED |
||
|
5 |
0 |
RW |
Y |
XPNT_SLAVE |
Always configure this bit to be master. Master control is assigned by mux selection 1: Channel is a slave 0: Channel is a master (recommended) |
|
|
4 |
0 |
RW |
Y |
XPNT_EN |
1: Cross Point is enabled 0: Cross Point is disabled |
|
|
3 |
0 |
RW |
Y |
EQ_BUFFER_EN[1] |
Enable EQ output buffers: 00: Neither buffer in ON (not recommended) 01: Only local buffer is ON 10: Only multi-drive buffer is ON 11: Both buffers are ON |
|
|
2 |
1 |
RW |
Y |
EQ_BUFFER_EN[0] |
||
|
1 |
0 |
RW |
Y |
EQ_DATA_MUX_IN[1] |
Select EQ data and signal detect bus from one channel: 00: channel A 01: Channel B 10: Channel C 11: Channel D Channel A = 0,4,8,12 Channel B = 1,5,9,13 Channel C = 2,6,10,14 Channel D = 3,7,11,15 |
|
|
0 |
0 |
RW |
Y |
EQ_DATA_MUX_IN[0] |
||