This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: Deserializer holds SCL down and blocks I2C communication

Part Number: DS90UB948-Q1


I'm using serializer 949 connected to host and 948 on the other side. I read register I2C_CONTROL_2 to check FORWARD_CHANNEL_S EQUENCE_ERROR bit and In very rare cases deserializer pulls SCL down and there is no recover from that except reset. BCC_WATCHDOG_CONTROL register has default values and I2C_CONTROL_2 register has the following configuration: I2C_BUS_TIMER_SPEED UP = 1,  I2C_BUS_TIMER_DISABLE = 0. I though I2C watchdog will handle this case bit it doesn't. Is there any way to handle this scenario?