This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: AMSEL signal level question

Part Number: TPS65987D

Hi all:

Hi,I have a new design using the TPS65987D + HD3SS460 ,to achieve USB3.0 and DP display through Type-C interface。

There is a phenomenon, what could be the cause?
The premise is: AMSEL has External circuitry to pull-up 100k and pull-down 100k.
Here are the steps:
(1) do not connect the dock to Type-C interface, power on the motherboard, AMSEL = 0V.
(2) Connect the dock to the Type-C interface, ALSEL = 0V.
(3) Unplug the dock from the Type-C interface and test AMSEL = 1.6V.
It can be seen that (3) and (1) are the same physical / device connection status: do not connect the dock to Type-C interface,
But (3) AMSEL = 1.6V and (1) AMSEL = 0V are different.
Why is this happening?