Part Number: TCA9617B
Hi Sir,
My customer planning to design TCA9617B as an I2C isolation as below schematic and have couple questions as below,
Could you please help on it?
Thank you
1. Since P3V3_Edge power on earlier than P3V3_AUX and TCA9617B EN has internal pull up to VCCB = P3V3_AUX,
Is there any concern for Enable pin design in the period when VCCA is on but VCCB is not on? The Enable pin will be in the floating level in that stage.
2. If we change the VCCA= P3V3_AUX and VCCB=P3V3_Edge, then the channel will be on in the beginning before VCCA= P3V3_AUX on, is there any concern for this design?
3. Do we have any suggestion or limitation about the VCCA & VCCB power on sequence?
4. If we design two TCA9617B B side connect to each other, is it acceptable? should we have anything need to be aware?