Part Number: TCAN4551-Q1
Other Parts Discussed in Thread: TCAN4550-Q1, TCAN4550
Hello,
I would like you to confirm about following two.
Q1 Could you please tell me maximum data rate ?
According datasheet of TCAN4550-Q1(also 4551-Q1), there is following description.
1. TCAN4550-Q1 supports CAN FD data rates up to 8 Mbps it is recommended to use a 40MHz crystal
On the other hand, there is following description as well.
2. The recommended value for CLKIN or crystal is 40 MHz to meet CAN FD rates up to 5 Mbps data rates in order to support higher data throughout.
I'm confusing about which one is correct information.
Q2 If TCAN455X-Q1 support up to 8Mbps as data rate, which frequency should be used for OSC ?
("40MHz" is described for both 5Mbps and 8Mbps in current datasheet.)
Best Regards,