This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Query on Pull up resistors on I2C lines

Part Number: PCA9306

Hello Support,

Greetings!!!

We are using I2C level shifter PCA9306 for our design.

We followed the datasheet reference design.

CPU <3.3v term> -----3.3v bus-------+---------------+-----------<3.3v termination>---last 3.3V device

                                                              |                     |

                                                     Level shifter       3.3V device

                                                     1.8V device

Here, we have 3.3V as master and also have 3.3V devices and one 1.8V device connected via level shifter. 

In that case do we need to add pull up resistors on 1.8V I2C lines?

We already have pull up resistors on 3.3V I2C lines. Is that enough?

Please provide your suggestions.

Thanks & Regards,

Veeralakshmi