Part Number: TUSB4020BPHPEVM
I'm experimenting with the TUSB4020BPHPEVM Evaluation Module and I am wondering if there is a way to utilize the PWRCTL1 and PWRCTL2 features of this IC on windows 10. Is there are a way to toggle these pins via a windows 10 GUI as well as is there any API such that the same action can be performed via python?