Part Number: TLK10232
Since I can’t find any schematics on this development board I wanted to know if there is a connection between the SFP housing and the input. For example, my specific case would be to convert a 10GBASE-KR signal coming directly from a backplane. I have the backplane signals coming out from a VPX chassis to SMA connectors. I want to take those SMA connectors with the 10GBASE-KR signal and convert it to a fiber media through the SFP+ housing I see on the development board. I wasn't sure if this was possible.