Part Number: TPS65987D
There are four questions from customer.
1. When using TPS65987D, which is the direction of power supply / reception in the initial state?
Customer wants to keep receiving power in the initial state.
2. I would like to supply power to iPAD / iPhone / Android etc. from our product equipped with TPS65987D.Is it possible to set the power supply current by I2C from the CPU on our product to TPS65987D?
Specifically, I would like to specify 4 current values of 5mA at 500mA / 900mA / 1.5A / 3A from CPU.
(I think how to specify the current from the CPU to TPS65987D by I2C etc.Is it possible to set it in units of 50 mA? )
3. If a current exceeding the value specified by the CPU above flows to the iPAD / iPhone / Android connected to TYPE-C, will the TPS65987D limit the current?
What is the current limit range?
(For example, if the TPS65987D is set to 500mA, will the power supply be stopped if a current exceeding 1.xx times that flows?)
4. Isn't TPS65987D an issue with debounce? (Are you able to handle it?)
Kagawa