Part Number: DS90UB941AS-Q1
Hi all,
I would like to know how to consider the minimum pixel clock when symmetric splitting mode. When outputting the 2xWVGA (800x480, 60fps, 23MHz pixel clock), the input can satisfy the device minimum pixel clock of 25MHz. However, the output of the pixel clock of 23MHz and the both output data rates of 368.640Mbps when 16bit and 414.720Mbps when 18bit cannot satisfy the 875Mbps minimum which is written in datasheet 8.3.2. How can we manage this?
Regards,
RYO