Part Number: TLIN1028S-Q1
Hi Experts:
As the description of datasheet , the capacitor on the VCC (LDO out) should be 10uF in the case that no load to full load.
In my application, the LDO output of TLIN1028S is used to power the MCU .SO the start up sequence is ;
1) Supply the Vsup
2) LDO ramping up and power for the MCU
3) MCU start working when voltage meet the threshold
4) MCU enable the TLIN1028S by pulling high the EN pin
5) TLIN1028S start communicating.
In this kind of usage, can I used the smaller capacitor like below 4.7uF, because the cost of 10uF could make the BOM cost higher.