I wish to test if the Cable with e-marker profile 20V 5A can actually handle 100W with 2x TPS65982 EVM modules but testing stops every time at 20V 3A
I Have connected a 150W Dell Power adapter to a TPS65982-EVM with config ID# 7 and connected the USB-C 100W capabe cable to this TPS65982-EVM and the other end connected to the 2nd TPS65982-EVM with Config ID# 6.
Now when I use a dynamic load on this 2nd TPS65982EVM I can load it up to 20V 3A after this point the 2nd TPS65982-EVM turns off (LEDs turn off) when I check the Source capacities using the FTDM I am able to get a max PD profile of 20V 5A so in my opinion I should be able to load this setup accordingly. But at this point it fails everytime at 20V 3A.
Is there an additional step I need to do to get the TPS65982 EVM to switch from the default 20V 3A PD profile to the 20V 5A PD profile?