This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cosmin,
It is generally possible to connect an RS-232 transceiver to the same connector pins as an RS-485 transceiver as long as you have the ability on each device to disable its respective driver output (so that multiple active drivers don't contend with one another). An example of this is shown here:
http://www.ti.com/tool/TIDA-00540
Some things to be aware of are:
- An RS-232 transceiver's "RIN" input generally has a 5-kOhm input resistance that cannot be disabled. This can introduce some additional loading when placed on an RS-485 line.
- Most RS-485 transceivers do not support the +/- 25-V tolerance required of RS-232 inputs. This may not be a concern for a given application, since the vast majority of modern RS-232 drivers output a lower voltage range. If it is a concern, though, a higher-voltage-capable transceiver like SN65HVD21 could be used.
Regards,
Max