Part Number: ONET8501P
Dear TI,
my First Question is:
is the differential input realy like in the blockchart with 100Ohm terminated or is there a CML logic with both 50Ohm to VCC?
my second question:
Can I use the ONET with a single ended 50 Ohm matched input?
If yes, what todo with the other input, 50Ohm to VCC?
Regards,
Jim