Part Number: DS250DF810EVM
Other Parts Discussed in Thread: DS250DF810
Has anyone got the ds250DF810EVM or similar 28G part to CDR lock on 10.3125 G KR? The 10G I use is from a FPGA and can loop back to itself through the same wires I use for the EVM board. The FPGA loopback does better than 1E-15 BER. When I bring those wires to the EVM it gets a signal detect but hardly ever a CDR lock. When I do an eye diagram at 400mv range it swamps screen with red with a very small opening in different places. It looks almost like I am not using 10.3125G but I verified it on the FPGA loopack with a Xilinx iBert. I tried reducing the output amplitude of the FPGA to 320mV thinking I was over equalizing but that did nothing. At 170mV output it lost signal detect so I would think that I did not over equalize it at 320mV. Any suggestions would be great. Thanks