Part Number: DP83867IR
Hi team
Datasheet 8.3.1 describes that a signal on GPIO is generated when qualifying signal is received in WoL configuration.
Could you explain more detail of the behavior of GPIO when magic packet is detected?
1. What is the initial state when DP83867 is waiting magic packet, low or high ?
2. When the magic packet is detected, how much is the duration of GPIO output?
3. Is this GPIO pin CMOS output or open-drain ?
Also, could you explain more detail of the behavior of GPIO when IEEE_1588_SFD_Tx and Rx is assigned to GPIO as well?
1. What is the initial state when DP83867 is waiting start-of-frame, low or high ?
2. When the start-of-frame is detected, how much is the duration of GPIO output?
3. Is this GPIO pin CMOS output or open-drain ?
Regards,
Saito