Part Number: TCAN1042H
Other Parts Discussed in Thread: TCAN1042-Q1
Hello, I see different supply current description in two TCAN1042 datasheet.
TCAN1042-Q1, sllses9c, 2019, Icc (dominant – with bus fault) max 110mA.
TCAN1042, SLLSES7C, 2017, Icc (dominant – with bus fault) max 180mA.
could you confirm if TCAN1042 non-Q1 has the same Icc with the Q1 110mA? SLLSES7C needs to update?
thanks.