This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987EVM: 10G-EXPANSION-EVM

Guru 29720 points

Part Number: TPS65987EVM

Hi Team,

I can't find product folder of 10G-EXPANSION-EVM.
It can be used with TPS65987EVM to confirm alternate mode function and I found the product folder in the past however can't find now.
Could you support it?

Best Regards,
Yaita

  • Hello Yaita,

    Unfortunately we took down the 10G-EXPANSION-EVM and will no longer ship them out. For an alternate modes such as DP, the PD controllers role is to negotiate and enter into the mode from the PD messaging standpoint, which can be verified using a PD analyzer. Apologies for the inconvenience.  

  • Hi Adam-san,

    It is regrettable to hear that.
    Can I hear the background of going out of production?
    It is just a simple question because I think the EVM is good tool to confirm alternate mode with TPS65987EVM.

    Best Regards,
    Yaita