This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Solution for portable screen

Team,

I need help finding a solution for the following requirements. The initial design was based off of the following TIDA: http://www.ti.com/tool/TIDA-03027#technicaldocuments

  1. UFP plug
    1. Display Port
    2. USB PD, 5V, 3A
    3. Communicates between a smartphone and USB 2.0 Hub
  1. DFP receptacle
    1. USB PD, 5V, 3A
    2. USB 2.0 HS
  1. DFP receptacle
    1. Display Port
    2. USB PD, 5V, 1A
  1. DFP plug
    1. Display Port
    2. USB PD, 5V, 1A
  • Hello Julio,

      Please elaborate on what the requirement is here.  Are you asking for just the power supply for each of these scenarios?  If so, one supply for all four?  Or are you asking for the interface to each of these?  Or both? 

    You stated the INITIAL design was based on the TIDA-03027; what has to be changed from that design? 

    Thanks,

    ~Leonard