Part Number: TCA5405
Other Parts Discussed in Thread: TS3DS10224, , TCA9534, TCA6408A
E2E,
I am looking for an I/O expander with at least 5 bits. The supply voltage is 3.6V, and I want to make sure that the VOH/VOL levels are compatible with the mux's (TS3DS10224) VIH/VIL.
I was looking at TCA5405, but I noticed that the VOH at 3.6V supply is 2.5V, which is lower than the VIH of the mux (shown below).
The min VIH is 0.75 x 3.6V = 2.7V.
Could you recommend an I/O expander with at least 5 bits that has a VOH larger than 2.7V?
Thank you!
Kate