Part Number: TUSB9261-Q1
Hi Team,
What is the low pulse width that the GRZ recognizes RESET surely?
That is, the minimum pulse width guaranteed by the device.
What happens if a shorter pulse is input?
For example, I want to know if it will not cause malfunction or destruction, if a short pulse is ignored and nothing happens, and what kinds of cases are possible.
I expect that a pulse slightly smaller than the guaranteed value will reset, but more smaller pulses will be ignored and nothing will happen.
The following is described in the power up and reset sequence of the data sheet.
A minimum reset duration of 1 ms is required. This is defined as the time when the power supplies are in the recommended operating range to the de-assertion of GRSTz.”
This means that the time from when the power supply stabilizes to when reset is released is at least 1 ms.
Is this correct?
Are there any restrictions on reset during power down?
Best regards,
Tomoaki Yoshida