Part Number: DS90UB954-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Hi peiyq,
The AEQ might be changing because there's unstable lock or parity errors in the link. I recommend running the Margin Analysis tool to check the eye margin of your system and set the best EQ range. Take a look at this app note: http://www.ti.com/lit/an/snla301/snla301.pdf
Best,
Jiashow
Hi Jiashow
I have ran the MAP tool to set the AEQ range (AEQ_MIN_MAX Address 0xD5) to 0xE0.
And I print AEQ_STATUS value (Address 0xD3).
Sometimes the AEQ_STATUS is 0xF or 0x17.
Why is AEQ_STATUS out of the AEQ range I set?
Hello,
You are setting your EQ level to 14.
From the AEQ_STATUS register, EQ Stage1 is bits 5:3, EQ Stage2 is bits 2:0.
Please refer to table 4 in the app note: http://www.ti.com/lit/an/snla301/snla301.pdf
Jiashow
Hi Jiashow
> From the AEQ_STATUS register, EQ Stage1 is bits 5:3, EQ Stage2 is bits 2:0.
> Please refer to table 4 in the app note: http://www.ti.com/lit/an/snla301/snla301.pdf
I have seen snla301 document.
I think that you mentioned is opposite.
For AEQ_STATUS register, EQ Stage2 is bits 5:3, EQ Stage1 is bits 2:0, is that right?
I can't find the document specification about this.
Could you show me that?
Hello,
I've verified with my team. For AEQ_STATUS register, EQ Stage2 is bits 5:3, EQ Stage1 is bits 2:0.
Jiashow
From our customer question, could you help to answer?
<Description>
Unexplained image cracking has occurred rarely. The log at that time is as attached (Please attach the log of # 5). AEQ_STATUS is incremented by a communication error,
and then a communication error occurs again and AEQ_STATUS is further incremented. This behavior makes AEQ_STATUS appear to be increasingly far from optimal.
Please answer the following questions.
<Question>
1. From the log, AEQ_STATUS appears to be transitioning to the Increment Inner Loop in Figure.5 if the error register is set even in the PowerOn state.
Although this route is not described in the Flow Chart, is there actually a route, and is this state transition correct?
2. Currently, the loop range is set to the full range 0 to F according to the recommendation of TI (Taiwan), but 0 to 5 is an appropriate range in TI Tool.
It seems wise to set this to 0-5 to avoid this phenomenon, is that correct?
Logcat as below shown:
Kernel_1970-01-01-09_00_35_356.log
01-01 09:00:54.232 0 0 I CAM_INFO: CAM-SENSOR: cam_sensor_driver_cmd: 1155 CAM_START_DEV Success, sensor_id:0x4688, sensor_slave_addr:0x6c
01-01 09:00:54.288 0 0 I CAM_INFO: CAM-SENSOR: cam_sensor_driver_cmd: 1155 CAM_START_DEV Success, sensor_id:0x2770, sensor_slave_addr:0x6c
01-01 09:00:56.958 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:00:56.959 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x2
01-01 09:00:56.959 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:56.959 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:00:56.991 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:57.018 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xE 0x4E=0xE5
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x4
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:57.021 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x1A
01-01 09:00:58.338 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:00:58.339 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x4
01-01 09:00:58.339 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:58.348 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:00:58.372 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:58.397 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:58.409 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x25
01-01 09:00:58.410 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x5
01-01 09:00:58.410 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:58.411 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x3C
01-01 09:00:59.618 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:00:59.619 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x5
01-01 09:00:59.620 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:59.621 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:00:59.656 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:59.678 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x4 0x4E=0x4
01-01 09:00:59.678 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x7
01-01 09:00:59.678 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:59.679 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x8
01-01 09:00:59.858 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:00:59.858 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x7
01-01 09:00:59.858 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:59.859 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:00:59.863 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:59.878 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:59.918 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x65
01-01 09:00:59.919 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0xF
01-01 09:00:59.919 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x7, STS2=0x4
01-01 09:00:59.920 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x1, RX_PAR_ERR_LO=0x3B
01-01 09:01:01.989 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:01:01.990 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0xF
01-01 09:01:01.990 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:01:01.992 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:01:02.045 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.052 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2871 CSID:1 ERROR_ECC
01-01 09:01:02.059 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.062 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x24
01-01 09:01:02.063 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x17
01-01 09:01:02.063 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x13, STS2=0x4
01-01 09:01:02.063 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:01:02.066 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.100 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.107 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2871 CSID:1 ERROR_ECC
01-01 09:01:02.114 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.118 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x65
01-01 09:01:02.118 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x1F
01-01 09:01:02.119 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x27, STS2=0x4
01-01 09:01:02.119 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x9, RX_PAR_ERR_LO=0xFC
01-01 09:01:02.136 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.151 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2871 CSID:1 ERROR_ECC
01-01 09:01:02.158 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.173 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:01:02.178 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x25
01-01 09:01:02.178 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x0
01-01 09:01:02.179 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x13, STS2=0x4
01-01 09:01:02.181 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:03:56.028 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0x0 0x4E=0x4
01-01 09:03:56.029 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x0
01-01 09:03:56.029 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:03:56.029 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x0
01-01 09:03:56.036 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2866 CSID:1 ERROR_CRC
01-01 09:03:56.088 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xF 0x4E=0x2
01-01 09:03:56.576 0 0 I CAM_INFO: CAM-SENSOR: cam_sensor_driver_cmd: 1189 CAM_STOP_DEV Success, sensor_id:0x4688, sensor_slave_addr:0x6c
01-01 09:03:56.743 0 0 I CAM_INFO: CAM-SENSOR: cam_sensor_driver_cmd: 1189 CAM_STOP_DEV Success, sensor_id:0x2770, sensor_slave_addr:0x6c
Hi Peiyq,
The AEQ range should be set based on the the MAP results. Has the customer run the MAP tool? Could you share the results?
Jiashow
Hello Jiashow,
Could you help to double check it? Map will be upload shortly.
In addition, could you help to confirm below screenshot ?
In this figure, it seems that only when powerup reaches AEQ stop, it will end. But in fact, after AEQ stop, if there are errors in the normal operation process, the log will continue to look for the appropriate EQ value.
Please help to confirm whether the flowchart should not go directly to the end after AEQ stop, but will wait. If there is an error, you will continue to adjust the EQ value (as seen from the log)
Hi peiyq,
You're right, AEQ will continue to check for errors even after it stabilizes.
The results look good to me, just make sure you set the EQ range based on the results.
Jiashow
Hi Jiashow,
Please help to update flow chart.
In additional, Could you let me know what the root cause for:
01-01 09:00:56.991 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:57.018 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xE 0x4E=0xE5
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x4
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1=0x3, STS2=0x4
01-01 09:00:57.021 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI=0x0, RX_PAR_ERR_LO=0x1A
What is the principle of this error? If the map value is good, why still have this problem? Is this kind of problem inevitable?
Hello,
It looks like you have some CSI errors. Could you check registers on 0x5C - 0x60 on the serializer side? Check the camera output if you are seeing CSI errors at the serializer.
Jiashow
Hi Peiyq,
Let me clarify, there's no errors on the SER error registers?
Which errors are you seeing on the DES side? Did you read registers 0x4D, 0x4E, 0x55, 0x56?
Best,
Jiashow
Hi Jiashow
> there's no errors on the SER error registers?
I have not read SER error registers (0x5C-0x60).
I checked the MIPI waveform with Oscilloscope.
> Which errors are you seeing on the DES side? Did you read registers 0x4D, 0x4E, 0x55, 0x56?
Yes, I read these registers. Following is the log.
01-01 09:00:56.991 0 0 E CAM_ERR : CAM-ISP: cam_ife_csid_irq: 2884 CSID:1 UNBOUNDED_FRAME
01-01 09:00:57.018 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 738 ov2718: ret=0, read 0x7A=0xE 0x4E=0xE5
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 763 ov2718: read DEVICE_STS=0xDF, AEQ_STATUS=0x4
01-01 09:00:57.019 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 767 ov2718: read STS1(0x4D)=0x3, STS2(0x4E)=0x4
01-01 09:00:57.021 0 0 I CAM_INFO: CAM-SENSOR: check_ds953_status: 771 ov2718: read RX_PAR_ERR_HI(0x55)=0x0, RX_PAR_ERR_LO(0x56)=0x1A
Hi peiyq,
After you initialize the system, could you first read 0x4D, 0x4E, 0x55, and 0x56 to clear any errors that may have occurred during initialization? And then you read the same registers again once you see flicker?
Right now it's hard to tell whether the errors in those registers are due to system initialization or the flicker.
Jiashow
Hello,
It looks like the issue is with the camera. Are you seeing CSI errors on the 953 side? When you use 953 pattern generation are you still seeing the same issues?