Part Number: SN65DSI83
Other Parts Discussed in Thread: SN65LVDS4, DSI-TUNER, SN65LVDS94
Hello,
We're using the SN65DSI83 in an application to convert i.MX 8M Mini DSI output to LVDS for a 7" 800x480 display. Our DSI clock frequency is 100.5 MHz and we have registers set to divide the clock by 3 to produce a 33.5 MHz output clock. The problem is that the output clock duty cycle is distorted to where the high pulse is ~58% and the low pulse is ~42%. This puts us near the specified limit of our panel and we think it may be causing some image quality issues we're seeing, particularly when the image is a mid-scale gray tone.
Is there any way to adjust the duty cycle of the LVDS output clock to be more symmetrical? We tried boosting the DSI clock so that we can divide by an even number, but that didn't affect the symmetry of the output clock at all.
Thanks,
Kevin Selle