Part Number: TPS65987DDJ
Hello,
I would like to know if I do a hard reset on the component it will reload the config from the SPI ?
Also which command I can do to re read the SPI configuration ?
best regards.
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987DDJ
Hello,
I would like to know if I do a hard reset on the component it will reload the config from the SPI ?
Also which command I can do to re read the SPI configuration ?
best regards.
David
Hello David,
Yes, whenever the device resets (remove power from VIN_3V3 or VBUS in dead battery scenario), the PD controller will re load the configuration from the external SPI flash.
There is not need for a command as the PD controller will read the configuration from the SPI flash by default.