Part Number: DS90C241
Hi there,
I'd like to ask you a basic question about FPD-link/SerDes. I might be confused with the concept of resolution, but I don't understand how Camera SerDes and Display SerDes in TI portfolio are exactly different.
1. Are two of them basically compatible except for several devices with specific interface(e.g. DSI for display and CSI for camera)? I meant, for example, DS90C241 is classified in Camera SerDes in subfamily, but it still can be used for Display SerDes if it met resolution and data rate?
2. I need to classify the devices in terms of data rate. In Display SerDes, can I think (color depth) * (pixel clock) as approximate max data rate? I was about to classify them with which display size the serializer support (e.g. 2K (2880x1080), WUXGA (1920x1200), or 1080p60 (1920x1080) etc., but there are a lot of devices which don't describe this information explicitly.
3. Can I classify Camera SerDes in terms of data rate in the same way above? I was thinking it can be based on 1+/2+/... MP, but a lot of device don't describe it as well.
Thank you for your time.