Part Number: DS80PCI402
hi,
We know DS80PCI402 is ideal for x4 PCI-Express,but if it can be used for x 8 PCIe with two chips? & Why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS80PCI402
hi,
We know DS80PCI402 is ideal for x4 PCI-Express,but if it can be used for x 8 PCIe with two chips? & Why?
Hi Lifang,
The DS80PCI402 or any of our other DS80PCIxxx devices can be used together in wider PCIe x8 or x16 link widths.
Each channel of these devices detects a valid Rx Termination independently which allows for flexibility when the system configures the PCIe link. Otherwise these redrivers are unaware of the underlying PCIe protocol.
Regards,
Lee