This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0340: I can not find the device address info in the datasheet

Part Number: LMH0340

hello,

In the docunment <3 Gbps, HD, SD, DVB-ASI SDI Serializer and Cable Driver With LVDS Interface >(datasheet of lmh0340), page12

"REGISTER WRITE
To write a data value to a register in the SER, the host writes three bytes to the SER. The first byte is the device
address—the device address is a 7 bit value, and if writing to the SER the last bit (LSB) is set to ‘0’ to signify that
the operation is a write. The second byte written is the register address, and the third byte written is the data to
be written into the addressed register. If additional data writes are performed, the register address is
automatically incremented. At the end of the write cycle the host places the bus in the STOP state. "

But,I can not find other infos in the document, wath exactly value is the device value.would you pls tell me where can i find it

thanks