This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IF: LED_1 and SD connection

Part Number: DP83822IF


Hello,

I want to confirm about below note in datasheet.

---------------------

TI recommends connecting Signal Detect pin from the Optical Transceiver to the LED_1 pin and enable it using SD_EN bootstrap pin in 100BASE-FX mode. The LED_1 pin is not used in design and that, if the electrical link between the fiber module and the DP83822 is broken, disconnected or otherwise disrupted, the link will recover only by initiating a soft reset through MDIO/MDC interface.

---------------------

When SD signal doesn't connect LED_1 and link broken, RESET required for recovery link. DP83822 link status depends on SD signal status. This means above condition never occurs when SD signal connects to LED_1 even though bit error rate is worse as not maintain link condition. Because link status equals SD signal.

Does my understanding correct?

Best regards,

Toshihiro Watanabe

  • Hi Toshihiro,

    Signal detect is only used for the fiber transceiver so I am not sure you can say that it is equal to the link status.

    Thanks,

    Cecilia

  • Hello Cecelia-san,

    I understood below post says LINK status equals SD signal status, I mean LINK is established when SD is active, LINK is broken when SD is inactive.

    Do I understand incorrectly?

    Best regards,

    Toshihiro Watanabe

  • Hi Toshihiro-san,

    Yes that is making more sense now. The SD depends on the link established. 

    Thanks,

    Cecilia

  • Hello Cecilia-san,

    Please let us discuss below note in datasheet.

    "TI recommends connecting Signal Detect pin from the Optical Transceiver to the LED_1 pin and enable it using SD_EN bootstrap pin in 100BASE-FX mode. The LED_1 pin is not used in design and that, if the electrical link between the fiber module and the DP83822 is broken, disconnected or otherwise disrupted, the link will recover only by initiating a soft reset through MDIO/MDC interface."

    1) Above notification is when SD signal does not connect to LED_1  -> The customer connects SD signal to LED_1

    2) DP83822 fiber mode link status = SD signal logic.

    [Question]

    1) The customer connect SD and LED_1. Is there any scenario the customer need to apply software reset as mentioned the NOTE?

      -> The customer worries below scenario and the system got frozen which link doesn't recover like NOTE case occurs.

          "Optical power of opto module got weak very much. In this condition, Opto module BER got worse like DP83822IF can't keep LINK connection. in this case, SD is still high,  showing link established. DP83822IF will understand LINK is still established but link is hard to keep in communication level.  In this mode, in this condition, optical cable was removed, LINK is re-established automatically?"

    The above is complex situation. It is OK we can know if we don't need to worry about NOTE case if SD signal connects to LED_1, never needed software reset. 

    Best regards,

    Toshihiro Watanabe

  • I will have to confirm with our design team on your Question #1. 

    Thanks,

    Cecilia

  • Hello Watanabe-san,

    Thank you for your patience. It looks like there may have been a typo in the description for this Note. You will only need to do a soft reset if you do NOT connect SD pin to the fiber transceiver. This will recover the broken link. No reset is required if you have connected SD to PHY. 

    Thanks,

    Cecilia

  • Cecilia,

    Please let me follow up this and let me ask additional questions.

    Customer also has concerns that the link is disconnected when the optical signal quality is bad due to vibration, bad optical cable connection, bad eye pattern and bad bit error rate and so on. When disconnections happen like this, they are not sure how to detect the failures. Could you give any ideas to solve this concern?

    Regards,

    Noriyuki Takahashi 

  • Hello,

    Please refer to section 8.4.10 Cable Diagnostics for our cable diagnostic features.

    Thanks,

    Cecilia

  • Cecilia,

    It seems that 8.4.10 Cable Diagnostics is for 100BASE-Tx. Customer system needs to support 100BASE-FX.

    So, in case of 100BASE-FX, how can they do to solve the link disconnection concern?

    Regards,

    Noriyuki Takahashi

  • Cecilia,

    This is a kind reminder. 

    Could you give any comments?

    Regards,

    Noriyuki Takahashi

  • Hello Takahashi-san 

    For fiber, we do not have a way to detect the cause for signal loss from the examples that you had mentioned above, we only have signal detect. You are also able to measure the RX_ER count to identify any packet errors.

    Thanks,

    Cecilia