Part Number: DS90UB948-Q1
Hi Team,
May I ask whether 948 could connect with two touch ICs?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Amelie,
Is the touch controller an I2C slave interface? If so then yes - you can connect the 948 I2C bus to two different touch ICs as long as they have different I2C addresses.
Best Regards,
Casey
Hi Casey,
Yes, thanks for your reply.
So both touch IC 1 and touch IC 2 need to connect to 948 I2C ouput (SCK and SDA)?
Thanks for your reply.
Just one more question. Since customer could only setup one address.
Could they control two touch ICs by different way, one touch IC is I2C, another one is SPI to control.
Thanks again for your help!
Hello Amelie,
Yes, if the touch controller has SPI as well then you could use I2C for one and SPI for the other. Please see the 948 datasheet and the relevant serializer datasheet for information on how to configure for forward channel SPI.
Best Regards,
Casey