Part Number: TUSB320
1. Can the voltage and current supplied from the TYPE-C terminal of the PC ?
Customer assumes 5V/0.9A or 5V/1.5A.
2. Is it possible to detect when a product is connected to the PC's TYPE-A terminal?
TYPE-A/TYPE-C cables may be used.
3. Can TUSB320 detect that the current supplied from the TYPE-C terminal of the PC cannot be set?
Is there a notification if the PC can not be supplied even if it requests 5V/1.5A ?
Best regards,
Kagawa