Part Number: THVD2410
Hi
I have selected the THVD2410 for my design, I have a below requirement
1. I have master controller on my board with THVD2410 transciever.
2. Bus input/output should have protection for ESD-IEC 61000-4-2, ISO16050 Pulse a, b surge (50V, 100uS), 24V battery short
I can see , device compliance with ESD. but do i need to have addition circuit protection for surge and short circuit. If yes, please suggest the recommended circuit.
Thanks
Dinesh