Part Number: PCA9306
My customer has asked about the PCA9306 application. He's guiding his team in China on this design.
See attached for application circuit from our datasheet.
The master is on 3.3V side and the Vref1=1.8V is enabled much later than the 3.3V on the master side.
The EN/VREF2 is controlled by master (3.3V) and could be present before Vref1 =1.8V.
The engineers indicated having problems with operation on applying power to the circuit and after RESET of the circuit, specifically on turning on Vref1=1.8V rail.
When they increased the value of the series resistor to EN/VREF2 to 10k, they reported that the failures stopped.
As I understand, the 200k series resistor is there to limit current that would “leak” from Vref2 to Vref1.
Could you, please, provide the recommendation for the resistor value limits and potential dangers of not restricting the current to Vref2?
PCA9306 application question.pdf*I read the latest data sheet for the part and understand the reason for the limitations, but need a formal response from TI to share with the design team.