Part Number: DS280BR820
The DS280BR820 datasheet (September, 2016) indicates on p.9 that the Vsdat AC signal detect assert (ON) differential voltage threshold level is the "Minimum input peak-to-peak amplitude level at device pins required to assert signal detect. 25.78125 Gbps with PRBS7 pattern and 20 dB loss channel." The Vsddt parameter is its de-assert (OFF) companion parameter, similarly worded. Both make reference to the level "at the device pins", yet also specify a 20dB loss channel. If the amplitude of importance is that amplitude present at the device pins, what difference does it make what characteristics the channel might have? For that matter, what difference do the precise datarate and signal pattern make, since the signal detect circuitry is presumably sensitive mostly/only to the (lower-frequency) behavior of the energy content of the signal?