This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP142: How placement the repeater to between CPU and DP connector

Part Number: TDP142

Hello,

 

My customer is going to apply the repeater into current board as below connection.

And data rate is 5.4GHz.

 

CPU -> CAP -> CMC -> (ESD ->) Display port connector

**ESD is option.

 

CPU: processor

CAP: AC coupling as 0.1uF

ESD: ESD IC of TPD4E02B04DQAR

CMC: Common mode filter as TCM065S-120-2P-T201 (TDK)

 

Please advise us where does TDP142 into current design?

For example; TDP142 and ac coupling are placed before CMC as below, is it right?

  CPU-> CAP-> TDP142-> CAP-> (ESD->) CMC-> DP connector

 

Thanks,

Katsu