Part Number: DS90UB954-Q1
hi!
According to the datasheet of DS90UB954-Q1, The absolute maximum input voltage to the FPD_Links range from 1.35V to 2.75V. But in the Power over coaxial cable section, the coaxial cable voltage is pulled up to 9V! (VPOC_RX) and the same coaxial line feeds to the FPD Link lines just through a Coupling Capacitor. So my question is, Won't it destroy the DS90UB954-Q1 IC? since the data lines are pulled to a higher voltage than absolute maximum value.