Part Number: TPS65987DDJ
Hi Team,
If I used the TPS65987DDJ as power source only(5V/3A&20V/5A) , not used as power sink , in this case , it's OK if we tie PPHV_1 & PPHV_2 together , is that correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987DDJ
Hi Team,
If I used the TPS65987DDJ as power source only(5V/3A&20V/5A) , not used as power sink , in this case , it's OK if we tie PPHV_1 & PPHV_2 together , is that correct?
Hello Andy,
Are you wanting to use both power paths at the same time? If so , then yes you can connect the two power paths directly to one another and implement the Power DUO functionality. However, if you are only using one power path, then I would recommend connecting PPHV2 to GND
Hi Adam,
Noted, thanks for feedback , further question , if I connected PPHV_1 & PPHV_2 together, but I only used one power path , it should be still ok , however we recommend to connecting PPHV2 to GND in common , is that correct?
Hello,
Connecting PPHV1 and PPHV2 to one another goes out side the recommended configuration for the TPS65987DDJ. I do not believe it would be an issue, but to be 100% sure, would recommend following the directions form the datasheet, which is to connect PPHV2 to GND when unused