Part Number: TUSB212
Other Parts Discussed in Thread: TUSB211, TUSB216
Hi Team,
My customer is evaluate these two solution , and have below question to ask
1. Is there's any different between TUSB211 & TUSB212?
- TUSB212 add I2C interface and DC_Boost function
- TUSB212 has higher redriving capability 4M , TUSB211 is 2M.
- ICC(max) : TUSB212=30mA , TUSB211=20mA
- ESD HBM (Typ) (kV) : TUSB212 =2KV , TUSB211=3KV.
kindly help to address if there's other different between these two solution.
2. Are these two solution P2P?
per my assume , if customer not used I2C and DC_Boost function ,then yes. they are P2P.
please help to correct if I had wrong on above questions , thanks!