Part Number: LMH0002
I want to know that if LMH0002 can be used to transmit a single pulse over long distances(about 100 meters)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH0002
I want to know that if LMH0002 can be used to transmit a single pulse over long distances(about 100 meters)?
Greetings,
1). This depends on the receiver at the end of 100m cable. LMH0002 is just the transmitter and receiver on the other end needs to recover this pulse.
2). Please note LMH0002 is AC coupled to 75-ohm cable. Therefor there is a RC time constant due to AC coupling capacitance values and terminating impedance. This means pulse need to be less than this RC time constant.
Regards,, Nasser