Part Number: SN65HVD70
The data sheet shows it being available in the MSOP-10 3x3 mm package. I found it in the 10VSSOP which is 3x5 mm with the pin to pin length.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD70
The data sheet shows it being available in the MSOP-10 3x3 mm package. I found it in the 10VSSOP which is 3x5 mm with the pin to pin length.
Hi David,
Confusing as it may be, these are the same package. The dimensions given on the front page of the datasheet are for the "body size," meaning pin lengths are excluded. The packaging and orderable addendum at the end of the datasheet gives the detailed mechanical info showing the addition ~2 mm of pin length.
Regards,
Max
yes seems to imply leadless package. I order some to study the disabled current draw. This question is taken care of so thanks.