Other Parts Discussed in Thread: TUSB217, TUSB216
We have a USB 2.0 Device to Device communication link that has been experiencing signal quality problems. Our setup is shown below.
Board A has a USB 2.0 Hub. In the first configuration the communication link goes from Board A through a connector to Board B then to the cable and on to Board C and D where there is another Hub. Cable lengths vary from 0.5m to 3m. Note that all cables are detachable on both ends.
In the second configuration, the cable also has a Board E in the middle with another USB 2.0 Hub. In this case each side of the cable is 4m for a total of 8m with hub in the middle.
We have experienced signal quality issues particularly with the longer 8m cable.
Shown below are far end USB 2.0 eye diagrams for the USB 2.0 High Speed signals at Board A, Board E, and Board D with the 8m cable. These eye diagrams were measured at the Hub pins. The 5th eye diagram shows a cable that was by far worse than most we have seen but does represent an exceptionally bad signal quality situation.
Here is what the far end eye diagrams look like with 1m cable.
If we were to use the TUSB217 to open up the eye diagrams where would you recommend we put them? Do you think we could boost the worst eye diagram shown while still staying within compliance for the shorter cable lengths?
Thank you,
Ethan