Part Number: DS250DF230
Hi Team,
DS250DF230 datasheet shows the following about SMBus Switching Characteristics (Slave Mode).
tHD_DAT: 0.75ns (typ)
tSU_DAT: 100ns (typ)
Could you let me know these minimum value?
Best Regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
Hi Team,
DS250DF230 datasheet shows the following about SMBus Switching Characteristics (Slave Mode).
tHD_DAT: 0.75ns (typ)
tSU_DAT: 100ns (typ)
Could you let me know these minimum value?
Best Regards,
Yaita
Hi Yaita,
I've included below for ease of reference the corresponding AC electrical parameters spec table from SMBus. As seen below the typical values from the datasheet correspond to the minimum values from the spec. Though listed on typical column these limits represent the minimum values. As these timing parameters are not tested in production TI guidelines prevent us from listing them on the "minimum" column in the datasheet.
Table 2. SMBus AC specifications
|
Symbol |
Parameters |
100 kHz Class |
400 kHz Class |
1 MHz Class |
Units |
Comments |
|||||
|
Min |
Max |
Min |
Max |
Min |
Max |
||||||
|
fSMB |
SMBus Operating Frequency |
10 |
100 |
10 |
400 |
10 |
1000 |
kHz |
See Note 1 |
||
|
tBUF |
Bus free time between STOP and START Condition |
4.7 |
– |
1.3 |
– |
0.5 |
– |
µs |
|||
|
tHD:STA |
Hold time after (REPEATED) START Condition |
4.0 |
– |
0.6 |
– |
0.26 |
– |
µs |
After this period, the first clock is generated |
||
|
tSU:STA |
REPEATED START Condition setup time |
4.7 |
– |
0.6 |
– |
0.26 |
– |
µs |
|||
|
tSU:STO |
STOP Condition setup time |
4.0 |
– |
0.6 |
– |
0.26 |
– |
µs |
|||
|
tHD:DAT |
Data hold time |
0 |
– |
0 |
– |
0 |
– |
ns |
See Note 2 |
||
|
tSU:DAT |
Data setup time |
250 |
– |
100 |
– |
50 |
– |
ns |
|||
|
tTIMEOUT |
Detect clock low timeout |
25 |
35 |
25 |
35 |
25 |
35 |
ms |
See Note 3 |
||
|
tLOW |
Clock low period |
4.7 |
– |
1.3 |
– |
0.5 |
– |
µs |
|||
|
tHIGH |
Clock high period |
4.0 |
50 |
0.6 |
50 |
0.26 |
50 |
µs |
See Note 4 |
||
|
tLOW:SEXT |
Cumulative clock low extend time (slave device) |
– |
25 |
– |
25 |
– |
25 |
ms |
See Note 5 |
||
Cordially,
Rodrigo Natal
HSSC Applications Engineer