Part Number: TUSB8041
Hello everyone,
I have a specific question:
- Is it possible to output USB 2.0 and USB 3.0 signals simultaneously/ parallel?
For example:
IC1 is connected to Port 1 over USB 2.0 D+/D-.
IC2 is connected to Port 1 with USB3.0 to TX+-/RX+-.
If the above is possible, there are a few other questions:
2. is the following possible:
Additionally to USB 2.0 D+/D- (over Port 1 again), the USB 2.0 connector would use PWR/OC of Port 1 to "supply" the connector with 5V.
Like in the first scenario, IC2 is connected to Port 1 with USB3.0 to TX+-/RX+-.
3. What happens, if in the last scenario OC would be triggered and TUSB8041 "deactivates" the PWR pin? Is there still an active connection to IC2 over USB 3.0?
Kind regards,
Marion