Part Number: TPD2S703-Q1
Hi Sir,
I saw the datasheet mentioned TPD2S703-Q1 can support USB3.0 but from the characters table the bandwidth only 960MHz,
How about the performance of USB3.0 2.5GHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD2S703-Q1
Hi Sir,
I saw the datasheet mentioned TPD2S703-Q1 can support USB3.0 but from the characters table the bandwidth only 960MHz,
How about the performance of USB3.0 2.5GHz?
Hi Anne,
Thanks for your question, I will confirm this item later will feedback you soon, thanks!
Hi Anne,
The USB3.0 port will have 9 pin including "DP,DM,VBUS,GND ,RX+,RX-,TX+,TX-,GND_DRAIN".
This device support DP and DM channel ESD protection ,so the application list the US3.0.
Hi Michael,
Thanks for the feedback, and my customer is looking for the part which has same feature as TPD2S703-Q1 but support USB3.0 TX+/- & RX+/- short protect from Battery, Vbus and GND. And support Automotive spec.
Could you please help to suggest on it?
Thanks
Hi Anne,
I am sorry, our product line don't have the TX,RX ESD protection device at this moment.
You can search in the TI.com to checking whether TI have other suitable USB3.0 TX,RX ESD protection device.